Lockup with CW3.1 for HS08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lockup with CW3.1 for HS08

ソリューションへジャンプ
3,369件の閲覧回数
johnm
Contributor I
I am using a standard registered version of CW 3.1 for HCS08.
When using it the program will lock up completely, usually after a few minutes.
This happens even when just browsing code.  It happens pretty much every time
I use CW.  I am running Win XP SP1, but could possibly get SP2 installed if it may help.
Regards
John
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,464件の閲覧回数
J2MEJediMaster
Specialist I
Are you using a firewall? That's been known to cause some problems, particularly if you're using a floating license. Also, go to the bottom of this Web page, and try entering the search string "Codewarrior hang" (no quotes), and examine some of the threads on this subject.

---Tom

Message Edited by J2MEJediMaster on 2006-09-27 09:36 AM

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,465件の閲覧回数
J2MEJediMaster
Specialist I
Are you using a firewall? That's been known to cause some problems, particularly if you're using a floating license. Also, go to the bottom of this Web page, and try entering the search string "Codewarrior hang" (no quotes), and examine some of the threads on this subject.

---Tom

Message Edited by J2MEJediMaster on 2006-09-27 09:36 AM

0 件の賞賛
返信
2,464件の閲覧回数
Alban
Senior Contributor II
I had similar trouble on CW 4.5 for S12 which disappeared when I re-installed Symantec Anti-Virus.
Alban.