Linker finding multiple file entries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linker finding multiple file entries

Jump to solution
1,542 Views
GaryOlmstead
Senior Contributor I

I have several programs that have been working for some time, always linking properly.  Today, I suddenly started getting a message that complained that every file in the project was entered twice.  Sure enough, they were, even though there have been no significant changes in months.  I tried deleting the extra files from the Link Order tab, (leaving them on the Files tab) and now I get a Compile Failed message with no other explanation.  I added the files back in, but I still get the Compile Failed message.

 

I also now get a message that says

 

"INTERNAL ERROR at line 490: Unknown macro: "PECW_CompileOptionsGap" (file:Config\Compiler\MetrowerksHC12CC.chg)

Hint: The -BfaGapLimitBits0 complier option has been added to the current target."

 

At one point, I was getting a Warning: L1016 message, but that went away when the compiler failed message showed up.  I looked up L1016, but all it says is that files are listed twice in a list but that isn't true.

 

This is from CW for HCS12.

 

If it matters, I have recently been running a separate installation of CW for the DSP56K.  That program is working correctly.

 

Any suggestions?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
892 Views
GaryOlmstead
Senior Contributor I
It seems to have been a corrupted project file.  I guess the computer crashed with CW still open.  I copied a project file from a known good backup version, and it went away.

View solution in original post

0 Kudos
Reply
1 Reply
893 Views
GaryOlmstead
Senior Contributor I
It seems to have been a corrupted project file.  I guess the computer crashed with CW still open.  I copied a project file from a known good backup version, and it went away.
0 Kudos
Reply