Linker and BSP problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linker and BSP problem

2,083件の閲覧回数
kdavis
Contributor III

MCF54418, CW 3.8, CW 10.2

 

I am having a problem where code warrior is saying that functions from the BSP are undefined, though it compiles fine. This is only happening with the real time clock module in particular. What I am really lost on is that it is able to build the sample RTC project provided by freescale, but is unable to build in my own project, the error output and calling code are below

 

C:/Freescale/CW MCU v10.2/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error

>Undefined : "_rtc_init(unsigned long)"

>Referenced from "initRTC()" in

C:/Freescale/CW MCU v10.2/MCU/ColdFire_Tools/Command_Line_Tools/mwldmcf|Linker|Error

>Undefined : "_rtc_int_enable(unsigned long,unsigned long)"

>Referenced from "initRTC()" in

 

int initRTC() {   int temp = _rtc_init(RTC_INIT_FLAG_ENABLE);   //install our interrupt   install_interrupt();   _rtc_int_enable (TRUE, RTC_INT_MIN_MASK);   return temp; }   

 

Added error for other part Message was edited by: Kevin Davis

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

1,937件の閲覧回数
Cdn_aye
Senior Contributor I

Kevin

This may be obvious, but did you enable the RTCS in the user_config.h file, rebuild the bsp, psp etc? The linkage error usually means MQX didn't include the module. I have seen something similar in the MFS. We had to enable the shell or we had errors even though we don't use the shell.

Good luck

0 件の賞賛
返信

1,937件の閲覧回数
Monica
Senior Contributor III

Kevin,

How is the project going? was this suggestion helpful or did you find any other resolution?

We'd like to know :smileywink:

Regards!

0 件の賞賛
返信

1,937件の閲覧回数
dataScout
NXP Employee
NXP Employee

Hello,

Are you linking with the same libraries as the sample project provided by Freescale?

Regards

0 件の賞賛
返信