Linker Error L1100

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linker Error L1100

3,548 次查看
done78
Contributor I

Hello,

I have just imported a project developed with CW 6.3 in the new CW 10.0, using HCS08 Toolchain; when  I try to build it, I get a lot of linker errors, i list here below:

 

 

ERROR L1100: Segments .absSeg0 (0x0) and .absSeg183 (0x0) overlap

ERROR L1100: Segments .absSeg1 (0x1) and .absSeg184 (0x1) overlap

ERROR L1100: Segments .absSeg2 (0x2) and .absSeg185 (0x2) overlap

ERROR L1100: Segments .absSeg3 (0x3) and .absSeg186 (0x3) overlap

ERROR L1100: Segments .absSeg4 (0x4) and .absSeg187 (0x4) overlap

ERROR L1100: Segments .absSeg5 (0x5) and .absSeg188 (0x5) overlap

ERROR L1100: Segments .absSeg6 (0x6) and .absSeg189 (0x6) overlap

ERROR L1100: Segments .absSeg7 (0x7) and .absSeg190 (0x7) overlap

ERROR L1100: Segments .absSeg8 (0x8) and .absSeg191 (0x8) overlap

ERROR L1100: Segments .absSeg9 (0x9) and .absSeg192 (0x9) overlap

ERROR L1100: Segments .absSeg10 (0xA) and .absSeg193 (0xA) overlap

ERROR L1100: Segments .absSeg11 (0xB) and .absSeg194 (0xB) overlap

ERROR L1100: Segments .absSeg12 (0xC) and .absSeg195 (0xC) overlap

ERROR L1100: Segments .absSeg13 (0xD) and .absSeg196 (0xD) overlap

ERROR L1100: Segments .absSeg14 (0xE) and .absSeg197 (0xE) overlap

ERROR L1100: Segments .absSeg15 (0xF) and .absSeg198 (0xF) overlap

ERROR L1100: Segments .absSeg16 (0x10) and .absSeg199 (0x10) overlap

ERROR L1100: Segments .absSeg17 (0x11) and .absSeg200 (0x11) overlap

ERROR L1100: Segments .absSeg153 (0x12) and .absSeg336 (0x12) overlap

ERROR L1100: Segments .absSeg154 (0x14) and .absSeg337 (0x14) overlap

ERROR L1100: Segments .absSeg18 (0x16) and .absSeg201 (0x16) overlap

ERROR L1100: Segments .absSeg19 (0x17) and .absSeg202 (0x17) overlap

ERROR L1100: Segments .absSeg20 (0x18) and .absSeg203 (0x18) overlap

ERROR L1100: Segments .absSeg21 (0x19) and .absSeg204 (0x19) overlap

ERROR L1100: Segments .absSeg22 (0x1A) and .absSeg205 (0x1A) overlap

ERROR L1100: Segments .absSeg23 (0x1B) and .absSeg206 (0x1B) overlap

ERROR L1100: Segments .absSeg24 (0x1C) and .absSeg207 (0x1C) overlap

ERROR L1100: Segments .absSeg25 (0x1D) and .absSeg208 (0x1D) overlap

ERROR L1100: Segments .absSeg26 (0x1E) and .absSeg209 (0x1E) overlap

ERROR L1100: Segments .absSeg27 (0x1F) and .absSeg210 (0x1F) overlap

ERROR L1100: Segments .absSeg155 (0x20) and .absSeg338 (0x20) overlap

ERROR L1100: Segments .absSeg28 (0x22) and .absSeg211 (0x22) overlap

ERROR L1100: Segments .absSeg29 (0x23) and .absSeg212 (0x23) overlap

ERROR L1100: Segments .absSeg30 (0x24) and .absSeg213 (0x24) overlap

ERROR L1100: Segments .absSeg31 (0x25) and .absSeg214 (0x25) overlap

ERROR L1100: Segments .absSeg32 (0x26) and .absSeg215 (0x26) overlap

ERROR L1100: Segments .absSeg33 (0x27) and .absSeg216 (0x27) overlap

ERROR L1100: Segments .absSeg34 (0x28) and .absSeg217 (0x28) overlap

ERROR L1100: Segments .absSeg35 (0x29) and .absSeg218 (0x29) overlap

ERROR L1100: Segments .absSeg36 (0x2A) and .absSeg219 (0x2A) overlap

ERROR L1100: Segments .absSeg37 (0x2B) and .absSeg220 (0x2B) overlap

ERROR L1100: Segments .absSeg38 (0x2D) and .absSeg221 (0x2D) overlap

ERROR L1100: Segments .absSeg39 (0x2E) and .absSeg222 (0x2E) overlap

ERROR L1100: Segments .absSeg40 (0x2F) and .absSeg223 (0x2F) overlap

ERROR L1100: Segments .absSeg41 (0x30) and .absSeg224 (0x30) overlap

ERROR L1100: Segments .absSeg42 (0x31) and .absSeg225 (0x31) overlap

ERROR L1100: Segments .absSeg43 (0x32) and .absSeg226 (0x32) overlap

ERROR L1100: Segments .absSeg44 (0x33) and .absSeg227 (0x33) overlap

ERROR L1100: Segments .absSeg45 (0x34) and .absSeg228 (0x34) overlap

ERROR L1100: Segments .absSeg46 (0x35) and .absSeg229 (0x35) overlap

 

 

 

 

It seems OK to me; please can someone explain me which steps i should take to spot where the error is ?

Thanks!!

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

2,105 次查看
Lundin
Senior Contributor IV

Abs seg refers to variables allocated with the non-standard @ operator. Unless you used this operator in your own code, the error is most likely caused by the Codewarrior register maps. Perhaps somehow the registers are allocated twice?

 

The best solution around the problem is to avoid the crappy Codewarrior register maps entirely, they aren't written in valid C and completely non-portable.

 

0 项奖励
回复

2,105 次查看
done78
Contributor I

Thank you Lundin,

problem is that the project seemed to work correctly on CW 6.3; unluckily i can't use that version anymore since it doesn't run on Windows 7. I suspect it to be something gone wrong in importing the project in the new CW, might it be that ?

I didn't use the '@' operator, but ubluckily the problem seems to arise because of a third party library i have included in my project (a .lib file) and whose source code I'm not able to read. I really don't know....

 

0 项奖励
回复

2,105 次查看
Lundin
Senior Contributor IV

Yeah well... "importing projects" from older versions to newer versions have never worked flawlessly on any IDE, compiler or platform known to mankind.

 

Are you sure that library is written in pure ISO C?

 

 

0 项奖励
回复

2,105 次查看
CrasyCat
Specialist III

Hello

 

It looks like the I/O registers are defined twice using @ operator.

 

Check in your source code where you define 2 objects at address 0x00 for example.

 

Note you can remap this message to an information or directly disable it using the option -MsgSi1100 (Remap message to information) or MsgSd1100 (disable message).

 

CrasyCat

0 项奖励
回复