Line # display.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,488件の閲覧回数
tmyint
Contributor I
Is there a way to display line numbers at the left margin beginning at the top of the document? This is in CW V5.0. thanks.

Thm
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,461件の閲覧回数
CrasyCat
Specialist III

Hello

No this is not possible. Note that when you place the cursor on a specific line in an edit window, you can see the corresponding line number in the edit window status bar.

CrasCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,462件の閲覧回数
CrasyCat
Specialist III

Hello

No this is not possible. Note that when you place the cursor on a specific line in an edit window, you can see the corresponding line number in the edit window status bar.

CrasCat

0 件の賞賛
返信
2,461件の閲覧回数
GonzaloVictorio
Contributor I
That's bad...
 
In general I don't like that much Codewarior editor... they should take a look at the VS2005 editor and grab some ideas...
0 件の賞賛
返信