Library Project in CodeWarrior 10.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Library Project in CodeWarrior 10.2

ソリューションへジャンプ
3,476件の閲覧回数
georgschmidt
Contributor III

Hi,

 

i have trouble creating a library for Kinetis MCU in CodeWarrior 10.2.

 

My first attempt was to create a new project using the Bareboard project wizard. On the devices page there ist an Option to choose the Project Type/Output, but the Library-Option is greyed out. What is going wrong here?

 

The second attempt was to change the Linker Output Type to "Library". The project compiles successfully, but I don't get a lib file anyway.

 

Can anybody give me some hints?

 

Regards,

Georg

ラベル(1)
0 件の賞賛
返信
1 解決策
2,747件の閲覧回数
Teckna
Contributor V

Hi Georg,

CW 10.3 has been released a month ago: you can download it here.

Teckna

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,747件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Libaries are supported in the wizard with MC10.3 (final release). It was not yet in the 10.3 beta.

For the ARM gcc compiler, the needed steps are described here: A Library with ARM gcc and Eclipse | MCU on Eclipse

2,747件の閲覧回数
georgschmidt
Contributor III

Hi Erich,

thanks for your answer. I'm trying to use the tutorial you posted but have Problems with step 4. If I click the Artifact Type dropdown there is no entry, so I can't choose anything. Can you help me on this?

When will CW 10.3 final be released?

0 件の賞賛
返信
2,748件の閲覧回数
Teckna
Contributor V

Hi Georg,

CW 10.3 has been released a month ago: you can download it here.

Teckna

0 件の賞賛
返信
2,747件の閲覧回数
georgschmidt
Contributor III

Hi,

I finally downloaded CW 10.3, now my library works fine.

Thanks to both of you!

Georgs

0 件の賞賛
返信