Kinetis design studio Trace and Profile

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis design studio Trace and Profile

跳至解决方案
2,627 次查看
bataliero
Contributor III

Hi,

where is "Trace and Profile" tab in Kinetis Design Studio? In CodeWarrior it is places in Debug Configuration. That features are not supported in KDS?

 

I am using K60 - TWR_k60n512.

 

page13:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4506.pdf

http://blogs.freescale.com/wp-content/uploads/2011/09/figure-1-the-codewarrior-ide-trace-feature-dis...

标签 (1)
0 项奖励
回复
1 解答
1,733 次查看
BlackNight
NXP Employee
NXP Employee

The CodeWarrior Trace and Profiling are not part of Kinetis Design Studio.

Trace and Profiling are supported by commercial IDE's for Kinetis, see IDEs for Kinetis MCUs|Freescale

If you want to do trace/profiling (on a different level, with source instrumentation), then this might be useful for you:

Poor Man’s Trace: Free-of-Charge Function Entry/Exit Trace with GNU Tools | MCU on Eclipse

Code Coverage for Embedded Target with Eclipse, gcc and gcov | MCU on Eclipse

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,734 次查看
BlackNight
NXP Employee
NXP Employee

The CodeWarrior Trace and Profiling are not part of Kinetis Design Studio.

Trace and Profiling are supported by commercial IDE's for Kinetis, see IDEs for Kinetis MCUs|Freescale

If you want to do trace/profiling (on a different level, with source instrumentation), then this might be useful for you:

Poor Man’s Trace: Free-of-Charge Function Entry/Exit Trace with GNU Tools | MCU on Eclipse

Code Coverage for Embedded Target with Eclipse, gcc and gcov | MCU on Eclipse

Erich

0 项奖励
回复