Kinetis K70 debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K70 debugging

1,544 Views
juanmanuelpanie
Contributor II

Hi, I want to debug a Kinetis K70 example code that is provided in Codewarrior 10.6. Is it possible to debug it without the board? I mean to simulate it.

Labels (1)
1 Reply

1,371 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Juan Manuel:

Unfortunately, CodeWarrior does not support simulation for Kinetis devices, you need to have the hardware connected.


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------