JM Badge Board - Windows 7 Sensor Function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JM Badge Board - Windows 7 Sensor Function

ソリューションへジャンプ
2,282件の閲覧回数
Glyn
Contributor I

Hi,

 

I've just received the JM Badge Board Rev D.

 

My development machine runs Windows 7 Professional (64 bit) on an Intel Core i7 920 CPU.

 

I use Visual Studio 2010 Professional and have downloaded and installed the Microsoft Windows SDK for Windows 7 and .NET Framework 4 (May 2010).

 

Pressing E4 enables the board to control the cursor movement by tilting and mouse clicks using E1-3 as expected. This seems to be working ok.

 

However, when I select E8 twice to enter Windows 7 sensor mode the Badge Board generates random continuous input. The only way to stop it is to unplug the board. Once unplugged the physical keyboard acts as if the control key is being held down. The mouse keys also do not function normally. The JM Badge Board is not detected as a Windows 7 Sensor device.

 

Is this a known issue?

 

I bought the JM Badge Board so I could simulate input from a Windows Phone 7 Series device; I'm developing software for the 7 series mobile platorm using VS2010 and Expression Blend 4.

 

Can anybody give me some instructions on how to get the JM Badge Board recognised as a Windows 7 Sensor device please?

 

Many thanks,

 

Glyn.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,611件の閲覧回数
Glyn
Contributor I

I've 'fixed' the problem.

 

There is a little repetition in my solution as I'm not sure which step fixed the problem!

 

Starting point:

 

Visual Studio 2010 and Windows 7 and .Net Framework 4 SDK (May 2010) installed.

 

Open "Location and Other Sensors" in Control Panel

Connect JM Badge Board to USB
Press E4
Run SensorDriverInstaller.exe from the Windows 7 Sensor Development Kit
Disconnect  JM Badge Board

 

Connect JM Badge Board to USB
Press E5
Tilting the board should move the mouse cursor.
Run SensorDriverInstaller.exe from the Windows 7 Sensor Development Kit
Disconnect  JM Badge Board

 

Connect JM Badge Board to USB
Press E8
Run SensorDriverInstaller.exe from the Windows 7 Sensor Development Kit
Sensor Development Kit appears in "Location and Other Sensors" window
Select enabled

 

You now have a working Windows 7 Sensor board.

 

Share and Enjoy,

 

Glyn.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,612件の閲覧回数
Glyn
Contributor I

I've 'fixed' the problem.

 

There is a little repetition in my solution as I'm not sure which step fixed the problem!

 

Starting point:

 

Visual Studio 2010 and Windows 7 and .Net Framework 4 SDK (May 2010) installed.

 

Open "Location and Other Sensors" in Control Panel

Connect JM Badge Board to USB
Press E4
Run SensorDriverInstaller.exe from the Windows 7 Sensor Development Kit
Disconnect  JM Badge Board

 

Connect JM Badge Board to USB
Press E5
Tilting the board should move the mouse cursor.
Run SensorDriverInstaller.exe from the Windows 7 Sensor Development Kit
Disconnect  JM Badge Board

 

Connect JM Badge Board to USB
Press E8
Run SensorDriverInstaller.exe from the Windows 7 Sensor Development Kit
Sensor Development Kit appears in "Location and Other Sensors" window
Select enabled

 

You now have a working Windows 7 Sensor board.

 

Share and Enjoy,

 

Glyn.

 

0 件の賞賛
返信