Issues with the Burner

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues with the Burner

Jump to solution
4,926 Views
Saga
Contributor II
Hi to all... I just want to burn a .bin image file into de uC with the burner utility, do you know how can i do that? Thank you!
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,083 Views
peg
Senior Contributor IV
Hi,
 
See this thread:
 
You must have missed it in your search.
 
Regards
Peg
 

View solution in original post

0 Kudos
Reply
5 Replies
3,084 Views
peg
Senior Contributor IV
Hi,
 
See this thread:
 
You must have missed it in your search.
 
Regards
Peg
 
0 Kudos
Reply
3,083 Views
Saga
Contributor II
Oh ok... Thank you a lot... i do missed it :smileyhappy:

Is there anyway for the hiwave to close after it finish the programming routine?

Thank you.
0 Kudos
Reply
3,083 Views
CompilerGuru
NXP Employee
NXP Employee
The exit command closes it.

Daniel
0 Kudos
Reply
3,083 Views
Saga
Contributor II
Hi to all... I've seen the hiwave applications only works with the ABS files, right? Do you know how to burn s19 files directly? I've been unable to do that... Thank you
0 Kudos
Reply
3,083 Views
peg
Senior Contributor IV
Hi Saga,
 
The load command will accept s record files as input as well as ABS file (intel hex and elf as well).
You can just enter LOAD on the command line and use the file open dialogue presented or LOAD ? will give you the commands options. This will produce a script that is run by the P&E command line programmer component. Another more manual way is to use the Expert programmer mode selectable form the menu that is named as per your interface pod.
 
Regards
Peg
 
0 Kudos
Reply