Issues with the Burner

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues with the Burner

ソリューションへジャンプ
4,952件の閲覧回数
Saga
Contributor II
Hi to all... I just want to burn a .bin image file into de uC with the burner utility, do you know how can i do that? Thank you!
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,109件の閲覧回数
peg
Senior Contributor IV
Hi,
 
See this thread:
 
You must have missed it in your search.
 
Regards
Peg
 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
3,110件の閲覧回数
peg
Senior Contributor IV
Hi,
 
See this thread:
 
You must have missed it in your search.
 
Regards
Peg
 
0 件の賞賛
返信
3,109件の閲覧回数
Saga
Contributor II
Oh ok... Thank you a lot... i do missed it :smileyhappy:

Is there anyway for the hiwave to close after it finish the programming routine?

Thank you.
0 件の賞賛
返信
3,109件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
The exit command closes it.

Daniel
0 件の賞賛
返信
3,109件の閲覧回数
Saga
Contributor II
Hi to all... I've seen the hiwave applications only works with the ABS files, right? Do you know how to burn s19 files directly? I've been unable to do that... Thank you
0 件の賞賛
返信
3,109件の閲覧回数
peg
Senior Contributor IV
Hi Saga,
 
The load command will accept s record files as input as well as ABS file (intel hex and elf as well).
You can just enter LOAD on the command line and use the file open dialogue presented or LOAD ? will give you the commands options. This will produce a script that is run by the P&E command line programmer component. Another more manual way is to use the Expert programmer mode selectable form the menu that is named as per your interface pod.
 
Regards
Peg
 
0 件の賞賛
返信