Issue with Reserved range overlap

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue with Reserved range overlap

跳至解决方案
2,828 次查看
MWMinor
Contributor V

Hi

 

I have migrated my CW V10.6 tools to a new laptop. When I imported a design (Coldfire MCF51JM128 product design) from my old laptop ( which also was running V10.6) I successfully compiled the design but am failing to programme the devices on my custom board. The board was working with the old laptop, but now I get an error;

58958_58958.pngpastedImage_0.png

I'm not sure where the configuration file is stored/generated, can anyone help me please.

 

Thanks

 

Ken

标签 (1)
0 项奖励
回复
1 解答
2,696 次查看
BlackNight
NXP Employee
NXP Employee

The memory configuration file is usually stored inside <project>\Project_Settings\Debugger\*.mem

Erich

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,697 次查看
BlackNight
NXP Employee
NXP Employee

The memory configuration file is usually stored inside <project>\Project_Settings\Debugger\*.mem

Erich

0 项奖励
回复
2,695 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ken,

from the error screenshot, the error is on the memory configuration file. please refer with attached video to check your memory configuration file setting.

I also attach MCF51JM128.mem from my side.

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复