Issue running silent install of CodeWarrior for MCUs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Issue running silent install of CodeWarrior for MCUs

跳至解决方案
2,125 次查看
mobashar
Contributor I

I am trying to install CodeWarrior for MCUs (v11.1) using silent install.  I read on another forum that this can be done using /S switch, which does work.  the command i use is shown below.

Setup.exe /S /D=C:\NXP\CW_for_MCUs

But just after i run this command i get the following prompt that i must press "OK" for to get the install to proceed.  Once I press "OK" the install proceeds successfully.

mobashar_0-1625799052704.png

I wanted to know if there is a way that this prompt can be suppressed so the install runs without any user interaction.  I need this to be able to install CodeWarrior onto a docker where I will only have access to the command line (no GUI).

标记 (2)
0 项奖励
回复
1 解答
2,100 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, silent install is not supported since CW10.6 so it's not supported in CW11.

Best regards,

Felipe

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,101 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, silent install is not supported since CW10.6 so it's not supported in CW11.

Best regards,

Felipe

0 项奖励
回复