Issue running silent install of CodeWarrior for MCUs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue running silent install of CodeWarrior for MCUs

Jump to solution
2,104 Views
mobashar
Contributor I

I am trying to install CodeWarrior for MCUs (v11.1) using silent install.  I read on another forum that this can be done using /S switch, which does work.  the command i use is shown below.

Setup.exe /S /D=C:\NXP\CW_for_MCUs

But just after i run this command i get the following prompt that i must press "OK" for to get the install to proceed.  Once I press "OK" the install proceeds successfully.

mobashar_0-1625799052704.png

I wanted to know if there is a way that this prompt can be suppressed so the install runs without any user interaction.  I need this to be able to install CodeWarrior onto a docker where I will only have access to the command line (no GUI).

Tags (2)
0 Kudos
Reply
1 Solution
2,079 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, silent install is not supported since CW10.6 so it's not supported in CW11.

Best regards,

Felipe

View solution in original post

0 Kudos
Reply
1 Reply
2,080 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, silent install is not supported since CW10.6 so it's not supported in CW11.

Best regards,

Felipe

0 Kudos
Reply