Is there a way to import data from xls in the CW IDE.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there a way to import data from xls in the CW IDE.

跳至解决方案
1,102 次查看
ankur_kala
NXP Employee
NXP Employee

I have seen implementations like MCAT and Quickstart that do provide the utility, but they are supported on limited devices. I need to do some calculation in an xls and use the answers in software. I do not want to copy paste them time and again. Is there any utility/method that can help?

标签 (1)
0 项奖励
回复
1 解答
982 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Ankur

Eclipse CodeWarrior for MCU supports exporting trace data to Excel,  as well as the registers information.  But I cannot find a way to import the data into CodeWarrior from Excel. However, you can open Excel file directly in CodeWarrior,  just drag the file into IDE. Before  it, please make sure  that the "Allow in-place system editors" option is checked.

allow editors.png

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
983 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello Ankur

Eclipse CodeWarrior for MCU supports exporting trace data to Excel,  as well as the registers information.  But I cannot find a way to import the data into CodeWarrior from Excel. However, you can open Excel file directly in CodeWarrior,  just drag the file into IDE. Before  it, please make sure  that the "Allow in-place system editors" option is checked.

allow editors.png

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复