Is there a stdargs.h header file for CW 10.2?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there a stdargs.h header file for CW 10.2?

ソリューションへジャンプ
1,247件の閲覧回数
samsaprunoff
Contributor V

Good day all,

I was curious if there is a "stdargs.h" header file for CW 10.2?  I ask, as I have some legacy could that I would like to port and it uses stdarg.h within some of its routines.  I could go through it and re-write it, but was hoping that there was a stdargs.h that I could use.

 

Thanks in advance!

Cheers,

Sam

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,144件の閲覧回数
DerekLau
Contributor IV

There are stdarg.h (not stdargs.h) files under the subfolders of \Freescale\CW MCU v10.2\MCU.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,145件の閲覧回数
DerekLau
Contributor IV

There are stdarg.h (not stdargs.h) files under the subfolders of \Freescale\CW MCU v10.2\MCU.

0 件の賞賛
返信
1,144件の閲覧回数
samsaprunoff
Contributor V

Good day Derek,

Thanks for your response!  Indeed, I made a mistake in the header file name for some reason I added the "plural" version :smileyhappy:

Cheers,


Sam

0 件の賞賛
返信