Is it possible to read a file from FTP as blocks

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to read a file from FTP as blocks

ソリューションへジャンプ
1,471件の閲覧回数
sumishgeorgeche
Contributor II

I wanted to read a file from ftp. Currently it fetches the whole file from ftp and then stores it in RAM and then write it to the flash memory. I wanted to try reading a particular number of bytes of the file at a time store it in the RAM then write it to the flash, continue this action till the whole file is read. I'm using codewarrior MCF54416

ラベル(1)
0 件の賞賛
返信
1 解決策
1,300件の閲覧回数
scottm
Senior Contributor II

Sure you can.  How hard it is to get there from here depends on what protocol stack you're using and how much control it gives you.

For starters, it's going to be easier to do if the flash memory you're writing to isn't the flash memory you're executing code from.  I've had an MCF51JM128 update itself via USB (including the USB stack) with no intermediate storage to work with and it was not fun.

Are you running an RTOS?  Which one?  What FTP implementation are you using?  Worst case, you can write your own FTP client, but that's probably a little excessive.

If you're using an RTOS it might be easier to approach it from the file system side.  Your RTOS might already have a suitable driver, but you could make one that writes directly to flash and use that as the destination for the FTP client.

Scott

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,301件の閲覧回数
scottm
Senior Contributor II

Sure you can.  How hard it is to get there from here depends on what protocol stack you're using and how much control it gives you.

For starters, it's going to be easier to do if the flash memory you're writing to isn't the flash memory you're executing code from.  I've had an MCF51JM128 update itself via USB (including the USB stack) with no intermediate storage to work with and it was not fun.

Are you running an RTOS?  Which one?  What FTP implementation are you using?  Worst case, you can write your own FTP client, but that's probably a little excessive.

If you're using an RTOS it might be easier to approach it from the file system side.  Your RTOS might already have a suitable driver, but you could make one that writes directly to flash and use that as the destination for the FTP client.

Scott

0 件の賞賛
返信
1,300件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi George,

is this question related to this other thread?

I am using codewarrior MCF54416. How can I write a file read from FTP directly into the flash memory...

Thanks in advance!

Best Regards,

Carlos Mendoza

Technical Support Engineer

0 件の賞賛
返信