Interpreting/Understanding map file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interpreting/Understanding map file

9,895件の閲覧回数
beng_
Contributor III

I've recently switched to using Code Warrior. I'm looking at the .map file output, and I'm struggling to interpret some sections of it.

(I'm used to using IAR Embedded Workbench)

 

I know I'm running close to the limit of my target's code size. So I want to know:

  1. What my current Code Size is?
  2. Which area of the source is generating the largest output? (So I can target that area)

Looking at my .map file I can see it's telling me in the Memory Configuration section how much I've allocated to each area (m_text, m_data), but I already knew that because I can read that from the linker file. What I can't see is how much of each section is actually used.

 

Is there any documentation explaining the output in the .map file?

ラベル(1)
タグ(2)
2 返答(返信)

7,779件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Ben,

The linker .map file is indeed hard to read, and actually does not help much :-(.

a) The simplest way to know this is to use the size utility and have the size printed after the link phase. You have several ways. One is to use a post-build command in CodeWarrior:

Printing Code Size Information in Eclipse | MCU on Eclipse 

Or use the 'Print size' checkbox, see Code Size Information with gcc for ARM/Kinetis | MCU on Eclipse 

See text, data and bss: Code and Data Size Explained | MCU on Eclipse  for  a description of the format/data. If you want something like this:

Memory region         Used Size  Region Size  %age Used
   PROGRAM_FLASH:       40648 B         1 MB      3.88%
      SRAM:       25748 B       192 KB     13.10%

Then you need the latest GNU tools.

b) That depends a little with the GNU tools used. CodeWarrior uses older ones, and I think you have to list each file as described in Listing Code and Data Size for each Source File with GNU and Eclipse | MCU on Eclipse . Newer GNU tools as in Kinetis Design Studio accept wild cards.

I hope this helps,

Erich

7,779件の閲覧回数
beng_
Contributor III

Thanks - that may be what I'm after

0 件の賞賛
返信