Interfacing two MC9S12XEP100 using CAN MAX3050 interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing two MC9S12XEP100 using CAN MAX3050 interface

2,329 Views
harshal_pawar
Contributor III

I am working on establishing communication between two MC9S12XEP100 controllers using CAN MAX3050ASA interface.

Is there any sample code available for the same as per your protocol standards ?

Labels (1)
3 Replies

2,177 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Harshal,

I recommend you refer AN3034 for CAN design

https://www.nxp.com/docs/en/application-note/AN3034.pdf 

Software for AN3034 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,177 Views
harshal_pawar
Contributor III

Thanks for the help

0 Kudos
Reply

2,177 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 Kudos
Reply