Interfacing two MC9S12XEP100 using CAN MAX3050 interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Interfacing two MC9S12XEP100 using CAN MAX3050 interface

2,340件の閲覧回数
harshal_pawar
Contributor III

I am working on establishing communication between two MC9S12XEP100 controllers using CAN MAX3050ASA interface.

Is there any sample code available for the same as per your protocol standards ?

ラベル(1)
3 返答(返信)

2,188件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Harshal,

I recommend you refer AN3034 for CAN design

https://www.nxp.com/docs/en/application-note/AN3034.pdf 

Software for AN3034 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,188件の閲覧回数
harshal_pawar
Contributor III

Thanks for the help

0 件の賞賛
返信

2,188件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信