Installing codewarrior on Windows 8

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing codewarrior on Windows 8

1,310 Views
dominiquebeusca
Contributor I

I try to install 'CodeWarrior v6.3 for HCS08' on a Windows8 system in 'basic licence' and I have the error message '... not compatible with Windows XP 64-bit installations.'

Which is the good link for this system ?

Labels (1)
0 Kudos
Reply
1 Reply

1,029 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dominique,

For the HSC08, you can install the CW10.6.4,

New CodeWarrior for MCU v10.6.4 available

Refer to the release note , it support the Windows8 .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply