Install CW 5.9.0 in WinXP available for ALL users

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Install CW 5.9.0 in WinXP available for ALL users

跳至解决方案
4,036 次查看
r490
Contributor II
I've installed the Special Edition CW 5.9.0 as administrator.  It never asks if you want this to be just for the administrator or for everyone.  When a non-administrator logs in, it is in the list of programs, but is not recognized as installed.  If the user navigates down to the correct location, he can start it and run it, so it is not an issue of files not being open to the regular user. 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,810 次查看
r490
Contributor II

So, I have solved this (a bit of a kludge).  I temporarily made the non-administrative user an admin.  Then installed for him, and changed him back to a member of PowerUsers group.  Seems to work for now.

--- RAM

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,811 次查看
r490
Contributor II

So, I have solved this (a bit of a kludge).  I temporarily made the non-administrative user an admin.  Then installed for him, and changed him back to a member of PowerUsers group.  Seems to work for now.

--- RAM

0 项奖励
回复
2,810 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

it seems this was in issue in the InstallShield (the installation program) used in CW 5.9. To my understanding this has been resolved in CW 6.1 as this uses the new InstallShield which has resolved this.

 

BK

0 项奖励
回复
2,810 次查看
r490
Contributor II

Perhaps I've overlooked something, but the only edition I see for HCS12 family is 5.9;  the version 6.1 is for other chips, not the HCS12 family.  Someone please correct me if I'm wrong on this.  Also, is there a patch to fix this problem in 5.9 if it is a known issue?

 

-- RAM 

0 项奖励
回复
2,810 次查看
J2MEJediMaster
Specialist I

Version 5.9 is the IDE version, not the actual version of the tools. To get the tools version number, select Help > About Freescale CodeWarrior > Installed Products. If you downloaded the Special Edition of the HC12 tools recently, it has to be version 5. You might file a service request to have this installer feature fixed or added.

 

Also, when posting a question, remember to include the hardware target name (such as HC(S)08 or HCS12(C)) along with the version number.

 

---Tom

Message Edited by J2MEJediMaster on 2009-09-18 09:06 AM
0 项奖励
回复
2,810 次查看
BlackNight
NXP Employee
NXP Employee

Hi RAM,

I (wrongly) assumed you are using CW for MCU/HCS08. My reply was targeting to that product line, and not the S12 one.

 

BK

0 项奖励
回复