Initializing the PAD port

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Initializing the PAD port

跳至解决方案
4,094 次查看
Franky_TJ_
Contributor I
Hi,  i'm having trouble initializing the PAD  port  im trying to set PAD07,06,14 and 13 as outputs using the DDR1AD0_DDR1AD06 register, there are no error messages when i compile the proyect but it never does it. 
any help will be very apreciated 
thank you. 
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,542 次查看
CrasyCat
Specialist III
Hello
I would recommend that you submit a service request with our support department around that.
 
Make sure to specify which version of CodeWarrior you are using and to attach a sample project reproducing the trouble.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,541 次查看
CrasyCat
Specialist III

Hello

Which processor are you targeting (HC08, EPPC, ...)?
Can I see the actual source code?

Did you define your port register as volatile?

CrasyCat

0 项奖励
回复
2,541 次查看
Franky_TJ_
Contributor I
Yes all are as volatile..here is the source code. The AD0 port works fine, but the AD1 is the one with the problem
the Micro I'm Using MC9s12xdp512v2
unsigned char RTSCTS(unsigned char port)
{
DDR1AD0 = 0;         
DDR1AD0_DDR1AD02 = 0; //INPUT PAD02 [93]  CTS3
DDR1AD0_DDR1AD03 = 0; //INPUT PAD03 [95]  CTS2
DDR1AD0_DDR1AD04 = 0; //INPUT PAD04 [97]  CTS1
DDR1AD0_DDR1AD05 = 0; //INPUT PAD05 [99]  CTS0
DDR1AD0_DDR1AD06 = 1; //OUTPUT PAD06 [101]  RTS2
DDR1AD0_DDR1AD07 = 1; //OUTPUT PAD07 [103]  RTS0
//CONFIGURE AD1 PAD08~PAD23
            // PIN  PIN   PIN   PIN
          //    DIR  NAME  NUMBER DESIGNATION
ATD1DIEN1 = 0x00;
ATD1DIEN0 = 0x00;         
DDR1AD1_DDR1AD19  = 0; //INPUT PAD09 [92]  CD3
DDR1AD1_DDR1AD110 = 0; //INPUT PAD10 [94]  CD2
DDR1AD1_DDR1AD111 = 0; //INPUT PAD11 [96]  CD1
DDR1AD1_DDR1AD112 = 0; //INPUT PAD12 [98]  CD0
DDR1AD1_DDR1AD113 = 1; //OUTPUT PAD13 [100] RTS3
DDR1AD1_DDR1AD114 = 1; //OUTPUT PAD14 [102] RTS1
 
 
  //PT1AD0_PT1AD07  RTS0 -->75C06 --> RTS1
  //PT1AD1_PT1AD114  RTS1 -->75C06 --> RTS2
  //PT1AD0_PT1AD06  RTS2 -->75C06 --> RTS3
  //PT1AD1_PT1AD113  RTS3 -->75C06 --> RTS4
}

Message Edited by Franky_TJ_ on 2006-07-12 05:55 PM

Message Edited by Franky_TJ_ on 2006-07-12 06:17 PM

0 项奖励
回复
2,543 次查看
CrasyCat
Specialist III
Hello
I would recommend that you submit a service request with our support department around that.
 
Make sure to specify which version of CodeWarrior you are using and to attach a sample project reproducing the trouble.
 
CrasyCat
0 项奖励
回复