Incorrect toolchain selected, CW10.6.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Incorrect toolchain selected, CW10.6.

1,210件の閲覧回数
randenewberry
Contributor IV

We are using Codewarrior 10.6. The processor is MK20DX128VLH7, 64 pin package. Using Processor expert, C code, No I/O, ARM Toolchain when creating the project.

Creating a new project only provides for the 100 pin variant to choose from. I added the 64 pin part from the processor expert, this is when I get the message "Incorrect toolchain selected in the project settings. Please change your project setting to use 'ARM Toolchain' or change the selected Compiler".

 

How do I get the 64pin package to use the same Toolchain?

ラベル(1)
0 件の賞賛
返信
1 返信

966件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

I tired on CW10.6, but did not reproduce the problem. Did you select the same options with me?

Untitled.png

I attached the project which I have changed the CPU into 64-pin MK20DX128VLH7. It built well.

0 件の賞賛
返信