Import a project.wsd file though commandline?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import a project.wsd file though commandline?

ソリューションへジャンプ
1,772件の閲覧回数
rossrhone
Contributor III

Is there a way to import a Project file via command line argument in Codewarrior 10.4 microprocessors? Example I want to import a project.wsd file and then be able to build the entire workspace via command line.

 

Thanks,

Ross

ラベル(1)
0 件の賞賛
返信
1 解決策
1,639件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ross Rhone

It seems that you are getting help for this topic in this thread: How to change references by command line?


Have a great day,
Jorge Alcala

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,640件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ross Rhone

It seems that you are getting help for this topic in this thread: How to change references by command line?


Have a great day,
Jorge Alcala

0 件の賞賛
返信