ICD12 does not show USB for P&E USB-ML

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ICD12 does not show USB for P&E USB-ML

ソリューションへジャンプ
2,197件の閲覧回数
roland_arthaud
Contributor I

Hello,

 

I am using CW 3.1

I have applied patch  CW12_V3_1_ICD12_USB2_0_Sim_patch.exe

 

Checking with device manager, I can see the driver correctly installed for USB-ML-12 Rev C

 

Using hiwave, I can see the following license info:

 

HI404000 (metrowks, 2.000): HI-WAVE Engine (Single User License, DISK: 7842c6cb, registered)
HI491000 (metrowks, 2.000): Flash Programming Support (Single User License, DISK: 7842c6cb, registered)
HI407238 (metrowks, 3.100): HC12 P&E ICD Target (Single User License, DISK: 7842c6cb, registered)

 

But in the ICD-12 menu, the Connect menu only shows LPT1 and COM1, but not USB

and therefore fails to connect to the target.

 

Does it strike a cord to anybody?

 

thx, Roland.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,557件の閲覧回数
CrasyCat
Specialist III

Hello

 

Any reason why you could not upgrade to the latest release of CodeWarrior for HC12?

P&E USB-ML is supported directly out of the box there.

 

CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,558件の閲覧回数
CrasyCat
Specialist III

Hello

 

Any reason why you could not upgrade to the latest release of CodeWarrior for HC12?

P&E USB-ML is supported directly out of the box there.

 

CrasyCat

0 件の賞賛
返信