I want to assemble asm files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I want to assemble asm files

ソリューションへジャンプ
2,435件の閲覧回数
andrewdavis
Contributor I

I have many files that are in coded ASM. Will CodeWarrior assemble these files?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,262件の閲覧回数
Leojunin
Contributor IV

You must configure the CW as relocatable assembler, put all the files in the source folder, and add these to the project. Compile and ready.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,262件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

In addition to Daniel ...

With the project wizard File + New + BareBoard, for the Language and Build Tools Options you can select the Language.

The options available depends of the processors:

    DSC and S12Z: C, C++, Mixed C and ASM, ASM

    Coldfire: no option excepted to select C++

    Kinetis: C, C++ and ASM

    Qorivva: C and C++

    RS08: C and Relocatable Assembly (using linker)

    HCS08: C, C++ and Relocatable Assembly (using linker)

  

Regards


Have a great day,
Pascal
NXP Technical Support

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,263件の閲覧回数
Leojunin
Contributor IV

You must configure the CW as relocatable assembler, put all the files in the source folder, and add these to the project. Compile and ready.

0 件の賞賛
返信
2,262件の閲覧回数
andrewdavis
Contributor I

How do I configure CW as relocatable assembler?

Andrew

0 件の賞賛
返信
2,262件の閲覧回数
Leojunin
Contributor IV

Init CW

If init "Startup menu" select "Create new project"

if not let File > Startup dialog then select "Create new project"

Follow the steps

at a certain point will give you wondering language options:

C ++

C

assembler

relocatable assembler

select relocatable assembler

when you finish add your .asm file in the sources folder located within the project folder

Then in the project, right-click on the sources folder and choose Add Files

find the .asm files you want to add using the browser opens.

and ready.

0 件の賞賛
返信