You must configure the CW as relocatable assembler, put all the files in the source folder, and add these to the project. Compile and ready.
Hi,
In addition to Daniel ...
With the project wizard File + New + BareBoard, for the Language and Build Tools Options you can select the Language.
The options available depends of the processors:
DSC and S12Z: C, C++, Mixed C and ASM, ASM
Coldfire: no option excepted to select C++
Kinetis: C, C++ and ASM
Qorivva: C and C++
RS08: C and Relocatable Assembly (using linker)
HCS08: C, C++ and Relocatable Assembly (using linker)
Regards
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
You must configure the CW as relocatable assembler, put all the files in the source folder, and add these to the project. Compile and ready.
How do I configure CW as relocatable assembler?
Andrew
Init CW
If init "Startup menu" select "Create new project"
if not let File > Startup dialog then select "Create new project"
Follow the steps
at a certain point will give you wondering language options:
C ++
C
assembler
relocatable assembler
select relocatable assembler
when you finish add your .asm file in the sources folder located within the project folder
Then in the project, right-click on the sources folder and choose Add Files
find the .asm files you want to add using the browser opens.
and ready.