I haven’t notice any significant differences in the settings between them.
Only connection manager differs from each other.
The first one is ICD – Connection Manager from CW5.1 and the second one is PEMICRO Connection Manager and additionally it has an option Trim Control.
Both connection manager auto-detects the port, in this case DEMOQE and under Target CPU auto-detects HCS08 Processor and a reset line High but in PEMICRO is missing information of CPU Voltage. See attached user interface of both connection managers.
-bumar