I cannot get into debug mode in CW10.5 for my Kinetis K60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I cannot get into debug mode in CW10.5 for my Kinetis K60

Jump to solution
1,390 Views
mehdikarimibiuk
Contributor V

I have MK60DN512 VLL10 with mini jtag for my PnE FX multilink connector (balck one which says Rev.A) and I cannot get into debug mode with it.

 

My project is a bareboard project with ProcessorExpert.

 

What are the things and steps that I have to check in my CW 10.5 to make sure there is nothing wrong with my environment.

 

Are those mem and init.tcl files needed?

 

Please guide me with the steps that I should follow in CW10.5

 

 

Thanks

Labels (1)
1 Solution
1,206 Views
trytohelp
NXP Employee
NXP Employee

Hi Mehdi,

The problem/question is already investigated under:

      -> another thread mini jtag connection

      -> under the Service Request system 1-1323008641.

I've contacted the engineer working on the SR.

For the second thread, as you can see, my colleague Jorge Gonzalez posted a new answer the April 19th too.

Hope this will help you.

Regards

Pascal

View solution in original post

2 Replies
1,207 Views
trytohelp
NXP Employee
NXP Employee

Hi Mehdi,

The problem/question is already investigated under:

      -> another thread mini jtag connection

      -> under the Service Request system 1-1323008641.

I've contacted the engineer working on the SR.

For the second thread, as you can see, my colleague Jorge Gonzalez posted a new answer the April 19th too.

Hope this will help you.

Regards

Pascal

1,206 Views
mehdikarimibiuk
Contributor V

Thanks, the problem is resolved now. We had a large capacitor on the jtag reset signal. It was 10u. We reduced the cap to 1u and it can pull down the reset in time now this I can get into debug mode with no pain.

Cheers

Mehdi