How to use HIWAVE to save all the memory(programs) in MC9S12A256CPVE FLASH to my computer?thank you very much

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use HIWAVE to save all the memory(programs) in MC9S12A256CPVE FLASH to my computer?thank you very much

Jump to solution
2,278 Views
1326532996
Contributor I

2.pngHow to save all FLASH

 program to my computer become a file xx.s19 or xx.abs   thank you,I need all memory

in>SAVE 4000..7FFF DUMP.s19
Error: bad digit in decimal numbe

 why is that?3.png

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,735 Views
BlackNight
NXP Employee
NXP Employee

You have to use 0x as prefix for hexadecimal numbers:

SAVE 0x4000..0x7FFF DUMP.s19

I hope this helps,

Erich

View solution in original post

2 Replies
1,736 Views
BlackNight
NXP Employee
NXP Employee

You have to use 0x as prefix for hexadecimal numbers:

SAVE 0x4000..0x7FFF DUMP.s19

I hope this helps,

Erich

1,735 Views
1326532996
Contributor I

Hi  Erich

Thank you for answering my question!I have solved the problem

But there was an error when save the third paragraph4.jpgError: while reading memory from 30C000
Reason: memory not defined in given range

How to solve?

0 Kudos
Reply