How to change the source file location?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the source file location?

1,157件の閲覧回数
danielchai
Senior Contributor I

Hi,

 

When I create a new source file in a project, it will create a xxx.c under the current folder.

How could I set the CW10.4 so that when I create the source file, it will create it in specific folder?

 

Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,069件の閲覧回数
BlackNight
NXP Employee
NXP Employee

It will use the folder you right click on as the default.

If you want to use a specific folder, either type the path or use the browse folder:

new file.png