How to address Segments_display Component to QY4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to address Segments_display Component to QY4

跳至解决方案
4,955 次查看
ecoli
Contributor I
I can't find a way to address the Segments_display on a Demo CodeWarrior 5.7.

The segments will be commanded trough PORTB, and de digits trough PORTA.

The Visualizationtool 7 Segment Display works ok, but I need more digits (and multiplexed, like it will be in real life).

If anybody can help me, I apreciate. Tks.

ecoli
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,253 次查看
BlackNight
NXP Employee
NXP Employee
Hello,
I fear there will be no simple answer.
The segments_display you can configure a little bit, but as you say: this does not provide you much what you want.
The 7-segment in the Visualisation tool is more generic (you can add more/etc), but is not multiplexed.

I think the only real solution is following: there is a product/package called 'Peripheral Builder', which allows you to create your own visualisation/peripherals. Basically it is an SDK, providing examples and wizards for Visual Studio (it was done for version 6.0). Teh 'segments_display' one was done with this SDK as an example, so you see what is possible. Now this would require some real C++ programming/etc to make it work.

Some more information: http://store.metrowerks.com/dr/v2/ec_Main.Entry17C?SID=43305&SP=10023&CID=145724&PID=699082&PN=1&V1=...

Erich

Message Edited by Alban on 02-27-2006 10:47 AM

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,254 次查看
BlackNight
NXP Employee
NXP Employee
Hello,
I fear there will be no simple answer.
The segments_display you can configure a little bit, but as you say: this does not provide you much what you want.
The 7-segment in the Visualisation tool is more generic (you can add more/etc), but is not multiplexed.

I think the only real solution is following: there is a product/package called 'Peripheral Builder', which allows you to create your own visualisation/peripherals. Basically it is an SDK, providing examples and wizards for Visual Studio (it was done for version 6.0). Teh 'segments_display' one was done with this SDK as an example, so you see what is possible. Now this would require some real C++ programming/etc to make it work.

Some more information: http://store.metrowerks.com/dr/v2/ec_Main.Entry17C?SID=43305&SP=10023&CID=145724&PID=699082&PN=1&V1=...

Erich

Message Edited by Alban on 02-27-2006 10:47 AM

0 项奖励
回复
2,253 次查看
ecoli
Contributor I
First of all, thaks for your answer Erich. I'll a try a less expensive solution.

I'll make real display experiments.
0 项奖励
回复