How to add Int_Flash.ttf file?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add Int_Flash.ttf file?

ソリューションへジャンプ
1,832件の閲覧回数
danielchai
Senior Contributor I

Hi All,

I am debugging a demo project and edit some configuration in Int_Flash.ttf. But when I close, it ask me to "Save to framework only" or "Save to file". I choose "Save to framework only". But after that, the ttf file disappeared from my project list.

5407_5407.pngfile.png

My question is how could I find it and make it show in the project list?

 

Thank you.

 

-Daniel

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,744件の閲覧回数
trytohelp
NXP Employee
NXP Employee


Hi Daniel,

this dialog allows you to save the task to the Framework or in a file.

If the Framework only is selected, the task will be saved in the Task component only.

If you need a file you must select Save to File.

for details, please have a look to the Targeting Microcontrollers.pdf manual:

       19.3.11.3 Storing Task to File

Regards

Pascal

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,745件の閲覧回数
trytohelp
NXP Employee
NXP Employee


Hi Daniel,

this dialog allows you to save the task to the Framework or in a file.

If the Framework only is selected, the task will be saved in the Task component only.

If you need a file you must select Save to File.

for details, please have a look to the Targeting Microcontrollers.pdf manual:

       19.3.11.3 Storing Task to File

Regards

Pascal

0 件の賞賛
返信