How to add Int_Flash.ttf file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add Int_Flash.ttf file?

Jump to solution
1,231 Views
danielchai
Senior Contributor I

Hi All,

I am debugging a demo project and edit some configuration in Int_Flash.ttf. But when I close, it ask me to "Save to framework only" or "Save to file". I choose "Save to framework only". But after that, the ttf file disappeared from my project list.

5407_5407.pngfile.png

My question is how could I find it and make it show in the project list?

 

Thank you.

 

-Daniel

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,143 Views
trytohelp
NXP Employee
NXP Employee


Hi Daniel,

this dialog allows you to save the task to the Framework or in a file.

If the Framework only is selected, the task will be saved in the Task component only.

If you need a file you must select Save to File.

for details, please have a look to the Targeting Microcontrollers.pdf manual:

       19.3.11.3 Storing Task to File

Regards

Pascal

View solution in original post

0 Kudos
Reply
1 Reply
1,144 Views
trytohelp
NXP Employee
NXP Employee


Hi Daniel,

this dialog allows you to save the task to the Framework or in a file.

If the Framework only is selected, the task will be saved in the Task component only.

If you need a file you must select Save to File.

for details, please have a look to the Targeting Microcontrollers.pdf manual:

       19.3.11.3 Storing Task to File

Regards

Pascal

0 Kudos
Reply