How to acquire the path of file(use Batch Burner Language)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to acquire the path of file(use Batch Burner Language)

2,259 Views
明超戴
Contributor II

I am using batch burner to generate .bin file,now I want to acquire the path of file with bbl ,but I did not find the information,the command as follows.

baudRate: Baudrate for Serial Communication
busWidth: Data Bus Width
CLOSE: Close Open File or Communication Port
dataBit: Number of Data Bits
destination: Destination Offset
DO: For Loop Statement List
ECHO: Echo String onto Output Window
ELSE: Else Part of If Condition
END: For Loop End or If End
FOR: For Loop
format: Output Format
header: Header File for PROM Burner
IF: If Condition
len: Length to be Copied
OPENCOM: Open Output Communication Port
OPENFILE: Open Output File
origin: EEPROM Start Address
parity: Set Communication Parity
PAUSE: Wait until Key Pressed
SENDBYTE: Transfer Bytes
SENDWORD: Transfer Word
SLINELEN: SRecord Line Length
SRECORD: S-Record Type
swapByte: Swap Bytes
THEN: Statementlist for If Condition
TO: For Loop End Condition
undefByte: Fill Byte for Binary Files

There are not the related command which I need ,can you help me ?thank you!

Labels (1)
0 Kudos
Reply
6 Replies

2,113 Views
BlackNight
NXP Employee
NXP Employee

Hello,

You might have a look at S-Record Manipulation with GNU objcopy and Burner Utility | MCU on Eclipse .

To open the *destination* file you write something like this:

OPENFILE "Merge.S19"

To read from the *source* file you write something like this:

SENDBYTE 1 "Part1.S19"

I hope this helps,

Erich

0 Kudos
Reply

2,113 Views
明超戴
Contributor II

thank you for your help, I know how to generate  .bin file ,as follows:

OPENFILE "C:\Users\zjxt\Desktop\TCU\bin\TCU_SECTION2.bin"

format=binary

busWidth=1

undefByte=0xff

origin=0xD800

destination = 0

len=0x800

SENDBYTE 1 "C:\Users\zjxt\Desktop\TCU\bin\Project.abs"

origin=0xDF8000

destination = 0x000800

len=0x4000

SENDBYTE 1 "C:\Users\zjxt\Desktop\TCU\bin\Project.abs"

CLOSE

but I do not like to add the path every time,I want to use a parameter to get the path of .bll file and store the .bin file with this path.could you unstand my mean.I hope you can help me ,thank you ,Best regards.

0 Kudos
Reply

2,113 Views
trytohelp
NXP Employee
NXP Employee

Hi,

You're using CW for MCU v10.6.x and the burner.exe tool.

Am I right ?

This tool is used to generate a Srecord, IntelHex or binary file from an abs file.

The tool can be used in GUI or in command line.

The BBL file contains the burner configuration.

By default if you create an example for S08, a burner.bbl is included in the project.

When the application is built, the burner is launched at the end and will create the .s19 file.

This is an example:

'Executing target #5 test_burner.abs.s19'

'Invoking: S08 Burner'

"E:/Freescale/CW MCU v10.6.4/MCU/prog/burner" -ArgFile"test_burner.abs.args" -f="../Project_Settings/Linker_Files/burner.bbl" -env"ABS_FILE=test_burner.abs"

'Finished building: test_burner.abs.s19'

' '

By default you must define the bbl file used.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,113 Views
明超戴
Contributor II

CodeWarrior5.1 ,MCU is MC9S12XEP100

0 Kudos
Reply

2,113 Views
trytohelp
NXP Employee
NXP Employee

This is the similar for HC12 v5.1 too.

For my understanding if you call the burner in the folder contained the abs file is located (C:\Users\zjxt\Desktop\TCU\bin\) the generated file will be placed in same folder.

0 Kudos
Reply

2,113 Views
明超戴
Contributor II

thank you for  your help,my  environment is CodeWarrior 。I will try your solution,I just want to gain the path of file (xxx.bll)and generate .bin file which related the path which we get。thank you, Best regards!

0 Kudos
Reply