How to Verify the code in my MC9S08QE8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Verify the code in my MC9S08QE8

跳至解决方案
1,475 次查看
rlstraney
Contributor III

Sorry to ask such a very simple question:

 

I have the P&E Multilink USB-ML-12E connected to my board and it works.  Now I need to know how to verify code that is on the board.

 

Background:  I downloaded code into my  MC9S08QE8 a couple months ago.   Now I want to go back and compile the source code I have and make sure it was the source code that generated what I downloaded into the MC9S08QE8 at that time.

 

I do not want to download the code I am now compiling - just verify that it matches what is in the chip.   I am using codewarrior V10.

 

How do I do this?

 

Renee

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,201 次查看
CrasyCat
Specialist III

Hello

 

Did you consider using a connect launch configuration and dumping memory content to a file.

 

In order to define a Connect launch configuration follow these steps:

 

    1- In CodeWarrior MCU V10 open the Debug Configuration dialog (Select Run > Debug Configuration).

    2- Click on CodeWarrior Connect on the left hand side of the dialog.

    3- Click on the New Launch Configuration icon to create a Connect Launch Configuration.

         This is the first icon to the left.

    4- In the main tab specify the Project and System the launch configuration applies to

    5- Specify a name for your launch configuration (this will be the name of the .launch file)

    6- Switch to the Common tab and check Shared file. Then browse for {ProjectDir}\Project_Settings\Debugger

        in the edit box.

    7- Click Apply. Your Connect Launch Configuration is created.

 

   Now Click debug to connect to your board. This should not erase the flash.

 

Once you are there you can open a Debugger shell view (Select Window > Show View > Other > Debug > Debugger Shell).

 

You can use the command SAVE to save content of memory as Motorola S record file.

 

Please refer to {Install}\MCU\Help|PDF\Targeting Microcontrollers.pdf manual, chapter Scripting, section Microcontrontrollers-Specific HIWARE Commands for more info about the syntax of this command.

 

Alternatively just type help save in the debugger shell view.

 

If you prefer using a GUI to dump memory content you can define a Target Task of type Import/Export/Fill memory to retrieve the content of memory.

 

There  are some information on target task in the Targeting Microcontrollers.pdf manual as well.

 

Search for Creating Target Task to Import Memory.

 

I hope this helps

 

CrasyCat

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,202 次查看
CrasyCat
Specialist III

Hello

 

Did you consider using a connect launch configuration and dumping memory content to a file.

 

In order to define a Connect launch configuration follow these steps:

 

    1- In CodeWarrior MCU V10 open the Debug Configuration dialog (Select Run > Debug Configuration).

    2- Click on CodeWarrior Connect on the left hand side of the dialog.

    3- Click on the New Launch Configuration icon to create a Connect Launch Configuration.

         This is the first icon to the left.

    4- In the main tab specify the Project and System the launch configuration applies to

    5- Specify a name for your launch configuration (this will be the name of the .launch file)

    6- Switch to the Common tab and check Shared file. Then browse for {ProjectDir}\Project_Settings\Debugger

        in the edit box.

    7- Click Apply. Your Connect Launch Configuration is created.

 

   Now Click debug to connect to your board. This should not erase the flash.

 

Once you are there you can open a Debugger shell view (Select Window > Show View > Other > Debug > Debugger Shell).

 

You can use the command SAVE to save content of memory as Motorola S record file.

 

Please refer to {Install}\MCU\Help|PDF\Targeting Microcontrollers.pdf manual, chapter Scripting, section Microcontrontrollers-Specific HIWARE Commands for more info about the syntax of this command.

 

Alternatively just type help save in the debugger shell view.

 

If you prefer using a GUI to dump memory content you can define a Target Task of type Import/Export/Fill memory to retrieve the content of memory.

 

There  are some information on target task in the Targeting Microcontrollers.pdf manual as well.

 

Search for Creating Target Task to Import Memory.

 

I hope this helps

 

CrasyCat

0 项奖励
回复
1,201 次查看
rlstraney
Contributor III

CrasyCat, 

 

Thank you for your reply on this matter.  Between your response and my research I finally figured out how to verify the code.   I was looking for a "verify" button but I quickly figured out it was a little more involved. 

Thanks Again,

 

Renee

 

0 项奖励
回复