How download code in TRK-KEA128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How download code in TRK-KEA128

2,004 Views
kuanyuenliao
Contributor II


Hello:

I use CW10.6, and download code to TRK-KEA128 by debug configurations (by OpenSDA), and do on-line testing for a while.

Now I need to keep the firmware when pull-out from debug, so I won't download every time when I want do a test. What options should I select in CW?

Thanks,

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

1,788 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kuan,

Do you want run the project without CW IDE.

If yes,

You needn't do nothing else , after you download your project into your

board, now ,you can re-insert the USB , it can work well , you can test one simple

project , for example hello world or LED demo .

If i misunderstand your meaning, please tell me .

Hope it helps!
Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,788 Views
kuanyuenliao
Contributor II

hello,

I have my easy project to play a blink LED on TRK-KEA128

when I use debug it works well, and press reset switch

then start at "__init_registers();" and resume also continue blink well.

Somehow, when I disconnect 未命名.png the debug (still keeping blink),

and then try press reset switch, then the led is never blink again.

that's why I say the code wasn't mount in the memory, and if any debug setting is necessary but I missed, please tell me, thank you

0 Kudos
Reply

1,788 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello KUAN,

I also create one simple LED project, and refer to your process to to , when

i did this process :
pastedImage_1.png

         the blue LED still blink .

      Please have a try .

Hope it helps!

ALice

0 Kudos
Reply