How do I rename a project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I rename a project

ソリューションへジャンプ
5,449件の閲覧回数
AndersJ
Contributor IV

CW 4.7 and 6.2. 

 

What is the correct way to rename a current project,

to make sure all files and folders are also renamed properly.

 

I believe I need to do a "Save Project As" but cannot find anything that seems to do this.

 

Thanks,

Anders J

ラベル(1)
タグ(1)
1 解決策
4,260件の閲覧回数
J2MEJediMaster
Specialist I

To rename a project and have it work, do the following:

 

1) Make a copy of your project folder (in case things go wrong, you can go back to original).

2) Change the copy's folder (the one holding the project files, especially the .mcp file) to the new project name.

3) Change the name of the .mcp file to the new project name.

4) Delete the folder OldProjectName_Data.

5) Open the newly named .mcp file with the CodeWarrior IDE.

6) Choose Project > Reset Project Entry Paths.

7) Choose Project > Re-search for Files. (These last two commands force the IDE to look for your source and other files by searching for them, and therefore will pick up the new directory path names.

 

You should be able to rebuild and use your project. Sorry, there is not a way to rename all of the source files automatically.

 

---Tom

元の投稿で解決策を見る

2 返答(返信)
4,261件の閲覧回数
J2MEJediMaster
Specialist I

To rename a project and have it work, do the following:

 

1) Make a copy of your project folder (in case things go wrong, you can go back to original).

2) Change the copy's folder (the one holding the project files, especially the .mcp file) to the new project name.

3) Change the name of the .mcp file to the new project name.

4) Delete the folder OldProjectName_Data.

5) Open the newly named .mcp file with the CodeWarrior IDE.

6) Choose Project > Reset Project Entry Paths.

7) Choose Project > Re-search for Files. (These last two commands force the IDE to look for your source and other files by searching for them, and therefore will pick up the new directory path names.

 

You should be able to rebuild and use your project. Sorry, there is not a way to rename all of the source files automatically.

 

---Tom

4,260件の閲覧回数
AndersJ
Contributor IV

Thanks Tom,

for a fine and detailed description of the renaming procedure.

Anders J

 

0 件の賞賛
返信