How do I add another chip architecture/type to CW10.6?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I add another chip architecture/type to CW10.6?

ソリューションへジャンプ
2,030件の閲覧回数
alager
Contributor II

When I start a new project my choices for device types are coldfire and kenetis.  I need to make an S08 project, how do I add this to my installation?

 

Thanks,

Aaron

ラベル(1)
0 件の賞賛
返信
1 解決策
1,947件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hi

It seems that you only selected Coldfire and Kinetis support packages when installing your CodeWarrior 10.6. Could you please also install the package for S08?

To install a new architecture later, you can use Install New Software and use the online update site. The link for the update site is:

http://freescale.com/lgfiles/updates/Eclipse/MCU10_6/com.freescale.mcu.updatesite

Please see this screenshot.

install new architecture.png

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,948件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hi

It seems that you only selected Coldfire and Kinetis support packages when installing your CodeWarrior 10.6. Could you please also install the package for S08?

To install a new architecture later, you can use Install New Software and use the online update site. The link for the update site is:

http://freescale.com/lgfiles/updates/Eclipse/MCU10_6/com.freescale.mcu.updatesite

Please see this screenshot.

install new architecture.png

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,947件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Aaron,

It also like the kinetis , when you create project , please select :

pastedImage_0.png

Does this can help you ?

BR

Alice

0 件の賞賛
返信