Hi! I am a beginner working with MM912_637

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi! I am a beginner working with MM912_637

2,628件の閲覧回数
mrunaljoshi
Contributor II

Hi! I am a beginner working with MM912_637 and I do not have the evaluation board but I am working with the assembled circuit for the IBS. What are the programming steps for MM912_637?

ラベル(1)
1 返信

2,324件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

Following the info I've found you can use CW for HC12 v5.1.

      CodeWarrior Dev Tools for HCS12(X) MCUs|Freescale

A patch must be installed to support MM913_637: CodeWarrior for HCS12(X) v5.1 MM912J637 Service Pack

For details please have a look to

      Battery Sensor with LIN for 12V Lead-acid Bat|Freescale

There are more information under the evaluation kit web page:

      http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KIT912J637EVME&fsrch=1

and the User Guide:

      http://cache.freescale.com/files/analog/doc/user_guide/KT912J637UG.pdf

Hope this will help you.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------