Help with debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,950件の閲覧回数
MathiasC
Contributor I
When I try to debug i get 101errors and 132warnings,
I use CW6.1 (on Vista)  and using target HC(s)08.
All errors and warnings referes to \ColdFire_support\msl\MSL_C\MSL_Common\Include\xxxx.h

xxxx.h  = mslGlobals.h or ansi_parms.h for example

Im new to using this software so please explain very carefully =)

/Mathias
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,932件の閲覧回数
CrasyCat
Specialist III
Hello
 
This question is not specific enough.
 
What sounds strange to me is you are telling you are building an application for HC08 and you are linking coldfire library to the application.
This cannot work.
 
I would suggest you to start with a brand new project. Use the project wizard to create your project and select the appropriate CPU & MCU from there.
 
This should fix all your problems.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,932件の閲覧回数
MathiasC
Contributor I
thanks for your help.

I will try that!

Im just trying to kick on an old project, and ive just followed the instructions

0 件の賞賛
返信
1,933件の閲覧回数
CrasyCat
Specialist III
Hello
 
This question is not specific enough.
 
What sounds strange to me is you are telling you are building an application for HC08 and you are linking coldfire library to the application.
This cannot work.
 
I would suggest you to start with a brand new project. Use the project wizard to create your project and select the appropriate CPU & MCU from there.
 
This should fix all your problems.
 
CrasyCat
0 件の賞賛
返信