HCS12 component / clock speeds, using CW 4.6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCS12 component / clock speeds, using CW 4.6

Jump to solution
1,766 Views
trav
Contributor III
I have a program to flash the LED component, but the LED's flash so fast that they start to blur or skip.  I've lowered the clock freq down to 1Hz and it's still too fast.  I'm using output compare for my delay and I have my delay routine set as slow as possiable.


I'm using CW4.6 for HCS12



J2MEJedi Master added MCU and CW version of subject line


Message Edited by J2MEJediMaster on 2007-09-14 10:38 AM
Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
789 Views
trav
Contributor III
I figured it out, I didn't have a device selected down in the bottom right corner of CW.

View solution in original post

0 Kudos
Reply
1 Reply
790 Views
trav
Contributor III
I figured it out, I didn't have a device selected down in the bottom right corner of CW.
0 Kudos
Reply