HCS12 component / clock speeds, using CW 4.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HCS12 component / clock speeds, using CW 4.6

跳至解决方案
1,748 次查看
trav
Contributor III
I have a program to flash the LED component, but the LED's flash so fast that they start to blur or skip.  I've lowered the clock freq down to 1Hz and it's still too fast.  I'm using output compare for my delay and I have my delay routine set as slow as possiable.


I'm using CW4.6 for HCS12



J2MEJedi Master added MCU and CW version of subject line


Message Edited by J2MEJediMaster on 2007-09-14 10:38 AM
标签 (1)
标记 (1)
0 项奖励
回复
1 解答
771 次查看
trav
Contributor III
I figured it out, I didn't have a device selected down in the bottom right corner of CW.

在原帖中查看解决方案

0 项奖励
回复
1 回复
772 次查看
trav
Contributor III
I figured it out, I didn't have a device selected down in the bottom right corner of CW.
0 项奖励
回复