HCS12 component / clock speeds, using CW 4.6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS12 component / clock speeds, using CW 4.6

ソリューションへジャンプ
1,802件の閲覧回数
trav
Contributor III
I have a program to flash the LED component, but the LED's flash so fast that they start to blur or skip.  I've lowered the clock freq down to 1Hz and it's still too fast.  I'm using output compare for my delay and I have my delay routine set as slow as possiable.


I'm using CW4.6 for HCS12



J2MEJedi Master added MCU and CW version of subject line


Message Edited by J2MEJediMaster on 2007-09-14 10:38 AM
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
825件の閲覧回数
trav
Contributor III
I figured it out, I didn't have a device selected down in the bottom right corner of CW.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
826件の閲覧回数
trav
Contributor III
I figured it out, I didn't have a device selected down in the bottom right corner of CW.
0 件の賞賛
返信