HCS12 Placing variables in EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS12 Placing variables in EEPROM

ソリューションへジャンプ
9,227件の閲覧回数
prog_ram
Contributor III

Hello,

I want to ask about placing variables in EERPOM for HCS12 - DP512.

1. The EEPROM manual states that the EEPROM is organaized in 16bits rows. Does that mean that I can't wirte one byte to certain memory location in EEPORM. Hence, I have to use 16bit pointers?. (I tried locating one byte in EEPORM, but CW didn't take it. Actually it compiled it but never located in EEPROM. It gave it just random address 0x0000!!).

 

2. In CW, when I flashed a value to EEPROM variable (using some functions I wrote), I counldn't verify that by looking at the memory map in CW (debug) as it doesn't reflect the new value of the EEPROM variable. I had to send it out via SCI to actually verify that the EEPROM has been seccussfully flashed. Any reasons/explanation/comments?

 

Thanks,

 

Prog_ram.. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,976件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello prog_ram,

 

did you really try to turn on the "Refresh memory when halting" option for the appropriate EEPROM item in the Debugging Memory Map window in the Debugger?

 

see e.g.

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=7585&query.id=1783#...

 

Stanish

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
4,976件の閲覧回数
J2MEJediMaster
Specialist I

Try looking at this thread for pointers on HCS12 EEPROM programming.

 

For viewing the EEPROM update, did you try Memory > Refresh in the Debugger?

 

---Tom

 

0 件の賞賛
返信
4,976件の閲覧回数
prog_ram
Contributor III

Hello Tom,

I don't have problems flashing data into the EEPROM. I am checking the word alignment and I am erasing a sector before wirting and all of that.. So far it seems to be working.

I couldn't be able to verify that the write function is working by checking the memory window in the debugger (I did the refresh, didn't show the udpate). I had to output the data via SCI to a terminal to verify that the variables in EEPROM have been updated..

 

It's just why the debugger doesn't show the udpate. If I am planning to flash unsigned int var[200] array into EEPROM, it's going to be defficult to output them all to a terminal to verify the successful flashing..

 

Here is my ee variables

#pragma DATA_SEG EE_DATA

 unsigned int ee_variable;

 unsigned int ee_variable1;

 unsigned int ee_variable2;

 unsigned int ee_variable3[2];

 float f_ee_variable;

#pragma DATA_SEG DEFAULT

 

and :

/* EPROM */

      EEPROM        = NO_INIT     0x0400 TO   0x07FF;

Placement: 

 EE_DATA        INTO EEPROM; 

 

One more thing.. please have a look at these statements and tell me if they are correct:

"The minimum data size that can be flashed into the EEPROM is 16bit (Word)."

 

"Any word can't be flashed before erasing the sector in which it's located. For this reason, the wirte function has to locate the sector address and erase it as the word in it maybe sector-aligned or not."

 

"Flashing data that is less than 16bit (a byte) will require extra job. Such as reading the current word (in which the new byte is located), and then flashing the whole word back again. This is true also for 4byte data where the whole sector has to be read/erased/flashed (in case the 4bytes cover just one sector, if not then two sectors have to be read/erased/flashed)."

 

Thanks for your support..

 

Prog_ram.. 

 

 

 

0 件の賞賛
返信
4,976件の閲覧回数
kef
Specialist I

prog_ram wrote:

 

"The minimum data size that can be flashed into the EEPROM is 16bit (Word)."

 That's right.

 

"Any word can't be flashed before erasing the sector in which it's located. For this reason, the wirte function has to locate the sector address and erase it as the word in it maybe sector-aligned or not."

Yes, but minimum erase size is whole 4-bytes/2-words sector. Sectors are sector-aligned of course.

 

"Flashing data that is less than 16bit (a byte) will require extra job. Such as reading the current word (in which the new byte is located), and then flashing the whole word back again. This is true also for 4byte data where the whole sector has to be read/erased/flashed (in case the 4bytes cover just one sector, if not then two sectors have to be read/erased/flashed)."

Yes, you read sector, change required bytes, then write sector back.

BTW, if you have plenty of spare EEPROM space, then you can reduce some overhead sector-aligning all your eeprom data, like this

 

/* EPROM */

      EEPROM        = NO_INIT     0x0400 TO   0x07FF ALIGN 4;

 

0 件の賞賛
返信
4,977件の閲覧回数
prog_ram
Contributor III

Thanks Kef for the verfication.. 

 

Still one issue remains, which is the CW Debugger not showing the udpated data in EEPROM as explained above..

 

what do you think the reason?

 

 

Regards,

 

Prog_ram.. 

0 件の賞賛
返信
4,977件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello prog_ram,

 

did you really try to turn on the "Refresh memory when halting" option for the appropriate EEPROM item in the Debugging Memory Map window in the Debugger?

 

see e.g.

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&message.id=7585&query.id=1783#...

 

Stanish

0 件の賞賛
返信
4,977件の閲覧回数
prog_ram
Contributor III

I tried it.. it's working!

 

thanks guys.. 

0 件の賞賛
返信
4,977件の閲覧回数
mati_qac
Contributor I

Hi everybody, i;ve tried to interfacing my MC9S12DG256MP with the internal EEPROM to write and read some important data. Unofortunately, i could not make that. I wanna know if somebody could help sending me a driver that already works

Thanks very much, my mail is [email protected] 

0 件の賞賛
返信
4,977件の閲覧回数
kef
Specialist I

Not a perfect solution for eeprom refresh trouble, but search box at bottom gave me this

http://forums.freescale.com/freescale/board/message?board.id=CW816COMM&message.id=326&query.id=28091...

 

So the way to update eeprom window is 

 

1. enter flash in command window 

 

   flash

 

2, then enter another command

 

   flash unselect

 

3. refresh memory window using context sensitive menu

 

Seems to work, though not very nice.

0 件の賞賛
返信