HCS08 TIM simulation problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCS08 TIM simulation problem

ソリューションへジャンプ
4,096件の閲覧回数
joerg
Contributor II
Hi
I try to simulate the output compare function for TIM1 of GB32/60, RC8 and QD4 MPUs.
But in the simulator the TIM does not trigger an interrupt. If i connect a MPU with the BDM it works just fine. The simulation of a TOF interrupt works in the full chip simulation. Is this a known problem (i noticed this behavior for CW3.1, CW3.2, CW5.0 and CW5.1!!)

Thanks Joerg

Message Edited by joerg on 2007-01-0112:30 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,530件の閲覧回数
CrasyCat
Specialist III
Hello
 
You need to submit a service request  for that.
This is an issue in P&E simulation module.  You can log that defect either with Freescale support or
directly with P&E.
 
To log the issue with Freescale please go to following URL:
and click on "Submit a service request"
 
To log the issue with P&E use following URL:
 
Note that Freescale support personal will anyway have to log that with P&E.
 
CrasyCat

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,531件の閲覧回数
CrasyCat
Specialist III
Hello
 
You need to submit a service request  for that.
This is an issue in P&E simulation module.  You can log that defect either with Freescale support or
directly with P&E.
 
To log the issue with Freescale please go to following URL:
and click on "Submit a service request"
 
To log the issue with P&E use following URL:
 
Note that Freescale support personal will anyway have to log that with P&E.
 
CrasyCat
0 件の賞賛
返信
2,530件の閲覧回数
joerg
Contributor II
Thanks CrazyCat
i have put the service request on the freescale support page:

ID: 1-335781881

Saluti Joerg
0 件の賞賛
返信
2,530件の閲覧回数
Phoenix
Contributor III
This bug will be fixed in v5.2 update patch. It should be released at the end of January.
0 件の賞賛
返信