HC12: memcmp() in CW is broken

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC12: memcmp() in CW is broken

5,329 Views
pittbull
Contributor III

Hello,
I'm using CW for S12X (IDE version 5.7.0.1714).
The memcmp() function does not work correctly.

Trying the below program on a Windows PC I get:
PASS!
PASS!
Code:

int my_memcmp_impl (void *s1, void *s2, unsigned int n){unsigned char *cs1 = s1;unsigned char *cs2 = s2;for (;n-- > 0; cs1++, cs2++)if (*cs1 != *cs2)return *cs1 - *cs2;return 0;}void test_memcmp (void){static unsigned char snonce[] = {0x0b, 0x97, 0x39, 0x0f, 0x37, 0x51, 0x78, 0x09, 0x81, 0x1e, 0xfd, 0x9c, 0x6e, 0x65, 0x94, 0x2b, 0x63, 0x2c, 0xe9, 0x53, 0x89, 0x38, 0x08, 0xba, 0x36, 0x0b, 0x03, 0x7c, 0xd1, 0x85, 0xe4, 0x14, };static unsigned char anonce[] = {0xd8, 0xa4, 0x80, 0x43, 0xb8, 0x37, 0x74, 0x02, 0xb9, 0x6a, 0xff, 0x49, 0xa5, 0x08, 0x9e, 0x93, 0x29, 0x37, 0x03, 0x47, 0x0e, 0xee, 0xa3, 0x17, 0xb4, 0x74, 0x30, 0xc6, 0xa6, 0x8d, 0x75, 0x2e, };debug_printf ("Testing memcmp (CW):\n");if (memcmp(snonce, anonce, sizeof(snonce)) > 0)debug_printf ("!!!! FAIL !!!!\n");elsedebug_printf ("PASS!\n");debug_printf ("Testing memcmp (my implementation):\n");if (my_memcmp_impl(snonce, anonce, sizeof(snonce)) > 0)debug_printf ("!!!! FAIL !!!!\n");elsedebug_printf ("PASS!\n");debug_printf ("\n");}


 
the same program running on an S12X target gives me
!!!! FAIL !!!!
PASS!

Message Edited by Alban on 2006-10-26 11:37 AM

Message Edited by CrasyCat on 2007-04-13 01:29 PM

Labels (1)
Tags (1)
0 Kudos
Reply
8 Replies

2,654 Views
CrasyCat
Specialist III
Hello
 
You have defined cs1 and cs2 as pointer to unsigned char.
 
When you are doing the operation *cs1 - *cs2, the operation is performed on unsigned value (no sign extension done prior to performing the operation).
 
If you define cs1 and cs2 as pointer to signed char, you get the expected FAIL message.
 
I hope this helps.
 
CrasyCat
0 Kudos
Reply

2,654 Views
pittbull
Contributor III
Hello,

From the C spec:
-----------------
7.21.4 Comparison functions
1 The sign of a nonzero value returned by the comparison functions memcmp, strcmp,
and strncmp is determined by the sign of the difference between the values of the first
pair of characters (both interpreted as unsigned char) that differ in the objects being
compared.

As you can see, my function does the right thing but the CW library uses 'signed' comparison (which is wrong according to the ISO/IEC document:smileywink:
0 Kudos
Reply

2,654 Views
Sten
Contributor IV
I agree with pittbull, it seems that CW does the memcmp() wrong.
I did a test on CW S12X v. 4.5 and when comparing two strings beginning with 0x0b and 0xd8, memcmp returns 0x33 which is a positive integer suggesting that 0x0b > 0xd8.
The right return value would have been 0xff35.

Message Edited by Sten on 2006-10-2603:33 PM

0 Kudos
Reply

2,654 Views
Lundin
Senior Contributor IV
I assume that you have this enabled:

Edit->Project settings->Type sizes-> char = signed

In ANSI C, the char type or may not be signed by default. On the other hand, one would have to assume that Metrowerks have adapted their function to suit the compiler's default char type.
0 Kudos
Reply

2,654 Views
pittbull
Contributor III
Lundin wrote:
In ANSI C, the char type or may not be signed by default.

Yes, it's implementation-defined but 'memcmp' must treat the input as unsigned...
0 Kudos
Reply

2,654 Views
CrasyCat
Specialist III
Hello
 
OK in that case submit a service request though our on line support web site.
This way the defect will be processed appropriately by our support team.
CrasyCat
0 Kudos
Reply

2,654 Views
pittbull
Contributor III
Hello CrasyCat,

CrasyCat wrote:
OK in that case submit a service request though our on line support web site....

Too late for me :smileymad:
This bad 'memcmp' caused a bug in a cryptographic function that was very hard to track down, but I already fixed it.
Nevertheless, I hope that one of the Freescale compiler folks find this thread and correct the library.
 
Cheers,
 -> pittbull

 
0 Kudos
Reply

2,654 Views
Lundin
Senior Contributor IV
Or simply write

return (int)*cs1 - (int)*cs2;
0 Kudos
Reply