HC12: Are there any differences between ansis.lib and ansisi.lib?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HC12: Are there any differences between ansis.lib and ansisi.lib?

跳至解决方案
3,284 次查看
tiny
Contributor I
hi:
The CW31 selected ansis.lib when I created a s12 project from stationery ,
but when i created the project using project wizard,it would choose the ansisi.lib as RTL

Message Edited by CrasyCat on 2007-04-13 01:39 PM

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,640 次查看
CrasyCat
Specialist III
Hello
 
The file {Install}\lib\HCI\readme.txt explains it a little bit.
 
 ansisi.lib   is used when you specify you want no floating point support. (option -D__NO_FLOAT__ )
 ansisf.lib   is used when you want to get float represented as 32-bit IEEE and double as 64-bit IEEE 
                  (option -Cf)
 ansis.lib    is used when you want to have both float and double represented as 32 bit IEEE.
 
As far as I can tell the 3 choices are available in the wizard for floating point support.
 
I hope this makes it a little bit clearer.
 
CrasyCat

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,640 次查看
tiny
Contributor I
oh...i see,thank you very much
0 项奖励
回复
1,640 次查看
tiny
Contributor I
thank you, cat
In small mode,
I noticed that CW31 would link ansisf.lib if float data type specified,and  ansisi.lib if not.
but the problem is in wich condition  would ansis.lib be used.
is ansis=ansisi+ansisf ?
0 项奖励
回复
1,641 次查看
CrasyCat
Specialist III
Hello
 
The file {Install}\lib\HCI\readme.txt explains it a little bit.
 
 ansisi.lib   is used when you specify you want no floating point support. (option -D__NO_FLOAT__ )
 ansisf.lib   is used when you want to get float represented as 32-bit IEEE and double as 64-bit IEEE 
                  (option -Cf)
 ansis.lib    is used when you want to have both float and double represented as 32 bit IEEE.
 
As far as I can tell the 3 choices are available in the wizard for floating point support.
 
I hope this makes it a little bit clearer.
 
CrasyCat
0 项奖励
回复
1,640 次查看
CrasyCat
Specialist III
Hello
 
If you specify floating point support as None and small memory model in the wizard,  ansisi.lib file will be linked to the application .
 
CrasyCat
0 项奖励
回复