HC12: Are there any differences between ansis.lib and ansisi.lib?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HC12: Are there any differences between ansis.lib and ansisi.lib?

Jump to solution
3,278 Views
tiny
Contributor I
hi:
The CW31 selected ansis.lib when I created a s12 project from stationery ,
but when i created the project using project wizard,it would choose the ansisi.lib as RTL

Message Edited by CrasyCat on 2007-04-13 01:39 PM

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,634 Views
CrasyCat
Specialist III
Hello
 
The file {Install}\lib\HCI\readme.txt explains it a little bit.
 
 ansisi.lib   is used when you specify you want no floating point support. (option -D__NO_FLOAT__ )
 ansisf.lib   is used when you want to get float represented as 32-bit IEEE and double as 64-bit IEEE 
                  (option -Cf)
 ansis.lib    is used when you want to have both float and double represented as 32 bit IEEE.
 
As far as I can tell the 3 choices are available in the wizard for floating point support.
 
I hope this makes it a little bit clearer.
 
CrasyCat

View solution in original post

0 Kudos
Reply
4 Replies
1,634 Views
tiny
Contributor I
oh...i see,thank you very much
0 Kudos
Reply
1,634 Views
tiny
Contributor I
thank you, cat
In small mode,
I noticed that CW31 would link ansisf.lib if float data type specified,and  ansisi.lib if not.
but the problem is in wich condition  would ansis.lib be used.
is ansis=ansisi+ansisf ?
0 Kudos
Reply
1,635 Views
CrasyCat
Specialist III
Hello
 
The file {Install}\lib\HCI\readme.txt explains it a little bit.
 
 ansisi.lib   is used when you specify you want no floating point support. (option -D__NO_FLOAT__ )
 ansisf.lib   is used when you want to get float represented as 32-bit IEEE and double as 64-bit IEEE 
                  (option -Cf)
 ansis.lib    is used when you want to have both float and double represented as 32 bit IEEE.
 
As far as I can tell the 3 choices are available in the wizard for floating point support.
 
I hope this makes it a little bit clearer.
 
CrasyCat
0 Kudos
Reply
1,634 Views
CrasyCat
Specialist III
Hello
 
If you specify floating point support as None and small memory model in the wizard,  ansisi.lib file will be linked to the application .
 
CrasyCat
0 Kudos
Reply